AXIS#.CANOPEN​.PERRMODE

Description

AXIS#.CANOPEN.PERRMODE can be used to configure the behavior of bit 13 of the DS402 statusword (6041h) in position error mode.

When AXIS#.CANOPEN.PERRMODE is set to 0, the statusword bit 13 will be set when F6001 (following error magnitude fault) is active.

When AXIS#.CANOPEN.PERRMODE is set to 1, the statusword bit 13 will also be set when W6001(following error magnitude warning) is active.

Versions

Action Version Notes
Implemented 02-03-01-000  

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
Stored in Non Volatile Memory Yes

Variants Supported

CAN bus drives: AKD2G-SPC

EtherCAT Drives: AKD2G-SPE

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.CANOPEN.PERRMODE

5003h

07h

Unsigned8

-

-

Read/Write

No